With more than 20 years of experience in run dry solutions, Regal Rexnord offers sustainable advantages for Can, PET or Glass production lines. Water and lubrication use for conveyor belts will be minimized with our premium DRY-PT™, advanced PSX® and Metal TableTop materials.
Thanks to Run Dry by Rexnord, conveyors save up to 9million liters of water and up to 27 thousand liters of lubricant each year.
Dry production floors and low noise levels help you achieve a safe working environment.
Minimal container damage and no unscheduled downtime will increase your productivity.
Without lubrication, conveyors are less sensitive to mold growth and allergic reactions to lubricants are eliminated.
Discover the Regal Rexnord Run Dry Concept for MatTop Chain
Read all about the benefits of converting to a dry production line.
Rexnord has committed years of research and development to bring the benefits of running dry to our Rexnord Metal TableTop portfolio which resulted in the Rexnord Dry Run 60 Series TableTop Chain. By focusing on specialized material development for the hinge of the Rexnord Run Dry 60 Series TableTop Chain, it can offer a run dry solution with the same dimensional properties as our legacy offering. This solution means there are minimal changes needed on the line to begin running dry. Installing and converting your line is as simple as replacing your old chain with the Rexnord Run Dry 60 Series TableTop Chain and then simply turn off the lubrication system.
Discover the Regal Rexnord Run Dry Concept for Metal TableTop Chain
Our Regal Rexnord Run Dry 60 Series is specifically designed to convert your Metal TableTop line to run dry
We understand that every production line and application within the Beverage Industry requires a different solution to convert to run dry. Depending on the type of application (Glass, Can or PET) or specific needs, Regal Rexnord will support you all the way!
What does it take to convert a glass line to run dry?
What does it take to convert a can line to run dry?
What does it take to convert a PET line to run dry?